Ame, a Sonepar Company in Spain, helped to deliver all kinds of electrical equipment for the expansion of the La Fe Hospital in Valencia.

Last week, Ame demonstrated the importance of proactivity during these challenging times. Their branch in in Puero de Sugunto helped to deliver all kinds of electrical equipment for the expansion of the La Fe Hospital in Valencia. The work was carried out in record time due to the urgency of the situation. Among the materials supplied by Ame, were signaling lights and the basic electrical installations needed for the smooth flow of medial activity.
Without support like this, frontline workers cannot carry out their work needed to fight this pandemic, and Ame is ready to do all they can to help. We’re in this together!
About Ame
AME (Almacén Material Eléctrico), was founded in January 1st, 2000, as a result of the merger of three companies: Comercial Antonio Chust (1925), Electro-Durá (1963) and Suministros Eléctricos Ferrer (1978). In 2011, AME Material Eléctrico joined Sonepar Ibérica. Ame is the leader in the Levante area of Spain. It currently has 24 branches with 330 associates and 30,000 items in stock.