Knowing that they were in a position to help, Sonepar Brazil OpCos raised funds in order to provide for areas in need.

The COVID-19 pandemic has been a highly challenging time for Brazil and has greatly impacted several communities in need. Knowing that they were in a position to help, Sonepar Brazil OpCos raised funds in order to provide for areas in need.
GDAIS, a volunteer group for Dimensional DW, came together to help the Brazilian Red Cross, by providing donations which were then used for the purchase of hygiene kits, information materials, and food packages.
Two other Sonepar Brazil OpCos, Nortel and Etil, joined local charities in the city of Campinas to collect donations which were used to provide food packages to more than 10,000 families without access to necessary resources.
Donations were able to be made through various channels in the Sonepar Brazil network, enabling associates and customers to contribute to these initiatives, reinforcing the belief that we are able to overcome times of crisis when we come together.
About Sonepar Brazil
Sonepar Brazil is part of the Sonepar Group, a global leader in the distribution of electrical materials. With operations in Brazil since 2001, it is also a leader in the national market and is constantly expanding its local presence through rapid growth and strategic acquisitions of companies in the segment. Currently, Sonepar Brazil is made up of the following companies: Dimensional, DW, Eletronor, Etil and Nortel.