The Cuevas del Drach are one of Mallorca’s biggest attractions, and Dieletro Balear is certain that this project will help to draw in even bigger crowds.

Dielectro Balear, a Sonepar company recently embarked on a project to renovate the lighting of the famous Cuevas del Drach (Caves of Drach) in Mallorca, alongside Signify. This was an extremely delicate and exciting project, as the first cave was first discovered in the Middle Ages and in the 19th Century, the French explorer and scientist Édouard-Alfred Martel discovered an underground lake which is connected to three more caves. The Cuevas del Drach are one of Mallorca’s biggest attractions, and Dieletro Balear is certain that this project will help to draw in even bigger crowds.
About Dielectro Balear
Dielectro Balear joined Sonepar Iberica in 2016 after establishing themselves as leaders in the market for the distribution of electrical equipment in the Baleric Islands. The company was founded in 1951 as part of the national Dielectro Group, until 1991, when it became Dielectro Balear. Currently, Dielectro Balear has five branches, over 110 associates, and more than 13,000 items in their warehouses.