Sonepar Italia has consolidated its wealth of knowledge to bring together an exciting partnership with Green Solution...

Sonepar Italia has consolidated its wealth of knowledge on digital solutions, electricity, lighting and renewable energy to bring together an exciting partnership with Green Solution, a company specializing in the installation and maintenance of electrical and photovoltaic systems.
Together, the two companies have constructed an innovative transport and photovoltaic system called the ‘People Mover’ in Bologna. This monorail runs purely on solar power and bridges the divide between Bologna airport and its train station at a speed of 40km per hour, connecting the two points in just seven minutes and 20 seconds.
About Sonepar Italia
Sonepar Italia is made up of 100 branches, five distribution centers and 1,500 associates. In 2018, Sonepar Italia generated a turnover of more than €600 million. Sonepar Italia was established in 1988 and prides itself on living by three principles: Closeness, Future and "La Référence".