This was a great project for KVC, whose primary goal is to help customers to build, operate, optimize and enhance their assets every day, and to offer other electrical solutions even in more harsh and hazardous environments.

 

On 6th July, KVC Industrial Supplies successfully assisted, one of the biggest oil and energy companies in Pahang, by upgrading the lighting in their plant to be completely explosion-proof. The lighting that KVC installed is the internationally recognized explosion-proof grade LED Linear light fittings solution by Crouse-Hinds.

Crouse-Hinds series HLL linear LED light fitting is constructed with an aluminum housing and high-impact resistant polycarbonate cover, providing extreme durability and reliability in Zone 1, 2, 21 and 22 hazardous areas. The use of high-quality LED chips, coupled with our extensive experience in thermal management of electrical components in hazardous areas, ensures long service life of the HLL series. The extended temperature range of -40 °C to +55 °C, allows these lights to be used in a wide range of ambient conditions where an explosive atmosphere is to be expected.

This was a great project for KVC, whose primary goal is to help customers to build, operate, optimize and enhance their assets every day, and to offer other electrical solutions even in more harsh and hazardous environments.

 

About KVC

KVC Industrial Supplies Sdn Bhd is a leading and growing Industrial supplier in Malaysia, founded in 1989. With their headquartered in Bangi, Selangor, they have more than 20 branches across Malaysia today, with approximately 600 associates helping to serve over 6,000 active customers.

Latest news Read all news