Sonepar and Signify Light Up the Cuevas del Drach in Mallorca

12.02.2021
2021.02.12 Dielectro Balear and Signify Light Up the Cuevas del Drach in Mallorca

The Cuevas del Drach are one of Mallorca’s biggest attractions, and Sonepar is certain that this project will help to draw in even bigger crowds.

Sonepar embarked on a project to renovate the lighting of the famous Cuevas del Drach (Caves of Drach) in Mallorca, alongside Signify. This was an extremely delicate and exciting project, as the first cave was first discovered in the Middle Ages and in the 19th Century, the French explorer and scientist Édouard-Alfred Martel discovered an underground lake which is connected to three more caves. The Cuevas del Drach are one of Mallorca’s biggest attractions, and Dieletro Balear is certain that this project will help to draw in even bigger crowds.